2014-05-28 11:20 AM
I am using the STM32F4 Discovery board with the Debug Port set to SW for the ST-Link debugger. Development is in stages, so I run STM32CubeMX to set a peripheral, debug the resulting code, then pull in another peripheral, lather, rinse, repeat. Every time I run CubeMX it resets the Debug port to JTAG. Is there a setting I missed -OR- is this a bug?
2014-05-29 7:28 AM
Hi,
This limitation is already fixed in STM32CubeMX V4.2.0You have just to update your STM32CubeMX tool version.With regards.2014-05-29 8:52 PM
I use v4.2. The problem is NOT fixed. Each time the project is regenerated, debug port (ST-Link) is reset to JTAG, not SW. Definitely a bug.
2014-05-30 1:53 AM
Which compiler toolchain are you using ?
2014-05-30 4:45 AM
2014-06-19 7:47 AM
Hello,
Indeed, after each code generation with MX, you will have to update the Keil uVision IDE debug configuration to use 'SW' instead of default 'JTAG'. This is a known limitation we're planning to fix in a future release. Best regards.2014-06-19 12:30 PM
Is there a bug list for MX?
2014-06-20 2:07 AM