2014-10-18 5:03 AM
Hi
I'm trying to use TCS3200 color sensor interface with stm32f4I used input capture of timer 2, channel 3 and Interrupt to calculator pulse from OUT sensorOf course, i don't know algorithm good. Because the sensor have 4 mode: blue, red, green and clear. One mode, we have a pulse another.i wrote as followvoid Color_filter(void) { /* Reset Sensor value */ RedMode = 1; GreenMode = 0; BlueMode = 0; TimeRed_H = 0; TimeRed_L = 0; TimeGreen_H=0; TimeGreen_L=0; TimeBlue_H=0; TimeBlue_L=0; /* Enable the CC3 Interrupt Request */ TIM_ITConfig(TIM2, TIM_IT_CC3, ENABLE); /* PB3--> S2, PB4--> S3*/ /* RED Filter */ GPIO_ResetBits(GPIOB,GPIO_Pin_3); GPIO_ResetBits(GPIOB,GPIO_Pin_4); Delay(1000); while(RedMode == 1); /* GREEN Filter */ GPIO_SetBits(GPIOB,GPIO_Pin_3); GPIO_SetBits(GPIOB,GPIO_Pin_4); GreenMode = 1; Delay(1000); while(GreenMode == 1); /* BLUE Filter */ GPIO_ResetBits(GPIOB,GPIO_Pin_3); GPIO_SetBits(GPIOB,GPIO_Pin_4); BlueMode = 1; Delay(1000); while(BlueMode == 1); /* Clear */ GPIO_SetBits(GPIOB,GPIO_Pin_3); GPIO_ResetBits(GPIOB,GPIO_Pin_4); /* Disable the CC3 Interrupt Request */ TIM_ITConfig(TIM2, TIM_IT_CC3, DISABLE); /* Timimg Calculation avoid for overflow */ if(TimeRed_H > TimeRed_L) TimeRed = (uint32_t)(TimeRed_H - TimeRed_L); else if(TimeRed_H < TimeRed_L) TimeRed = (uint32_t)((0xFFFF - TimeRed_L) + TimeRed_H); if(TimeGreen_H > TimeGreen_L) TimeGreen = (uint32_t)(TimeGreen_H - TimeGreen_L); else if(TimeGreen_H < TimeGreen_L) TimeGreen = (uint32_t)((0xFFFF - TimeGreen_L) + TimeGreen_H); if(TimeBlue_H > TimeBlue_L) TimeBlue = (uint32_t)(TimeBlue_H - TimeBlue_L); else if(TimeBlue_H < TimeBlue_L) TimeBlue = (uint32_t)((0xFFFF - TimeBlue_L) + TimeBlue_H); /* Frequency Calculation */ FreqRed = SystemCoreClock/TimeRed; FreqGreen = SystemCoreClock/TimeGreen; FreqBlue = SystemCoreClock/TimeBlue;}void Delay(__IO uint32_t nCount){ while(nCount--) { }}void TIM2_IRQHandler(void){ if(TIM_GetITStatus(TIM2,TIM_IT_CC3) == SET) { if((RedMode == 1) && (Number == 0)) { TimeRed_L = TIM_GetCapture3(TIM2); Number = 1; } else if((RedMode == 1) && (Number == 1)) { TimeRed_H = TIM_GetCapture3(TIM2); RedMode = 0; Number = 0; } else if((GreenMode == 1) && (Number == 0)) { TimeGreen_L = TIM_GetCapture3(TIM2); Number = 1; } else if((GreenMode == 1) && (Number == 1)) { TimeGreen_H = TIM_GetCapture3(TIM2); GreenMode = 0; Number = 0; } if((BlueMode == 1) && (Number == 0)) { TimeBlue_L = TIM_GetCapture3(TIM2); Number = 1; } else if((BlueMode == 1) && (Number == 1)) { TimeBlue_H = TIM_GetCapture3(TIM2); BlueMode = 0; Number = 0; } TIM_ClearITPendingBit(TIM2,TIM_IT_CC3); }}it gets stuck when coming out of interrupt in the first. i really hope you can give me one solution.2014-10-18 9:22 AM
Assume I don't want to read the datasheet for this TCS3200, describe the nature of the signal it generates and how this is attached to the STM32.
Assume I can't see the code you haven't presented, I don't therefore know how the timebase or channel are configured.