2016-07-01 1:36 PM
Hi Experts,
We would like to save some small amount of application data - about 100 bytes somewhere on the STM32L486 chip that will survive power down / power up cycle.Before, when we were using STM32L1, I had a very simple code that was writing to and reading from the EEPROM:// to save data: FLASH_UnlockData(); uint32 *pu32Nvm = (uint32*) ( 0x08080000 ); pu32Nvm[0] = ... some data ...; pu32Nvm[1] = ... some data ...; ... FLASH_LockData();// to read data: just read starting from 0x08080000.Is there a similar equivalent in the STM32L4 / Cube? #stm32l4-flash2016-07-02 2:38 PM
Nothing identical. Options that come to mind are:
1KB one time programmable (OTP) memory The same constant data in every application loaded Protecting a dedicated flash memory block Adding a battery and using backup RAM registers Cheers, Hal