cancel
Showing results for 
Search instead for 
Did you mean: 

reading the falsh content using JTAG

babidesai123
Associate II
Posted on January 09, 2004 at 14:52

reading the falsh content using JTAG

7 REPLIES 7
babidesai123
Associate II
Posted on May 17, 2011 at 11:53

Hi,

Can we read the flash memory (full or sector) using the JTAG programming??provided that flash sector is not protected.

if yes the what are the steps??

Can u give detail steps to read the flash mem content using JTAG?

[ This message was edited by: Purvi on 11-04-2003 08:54 ]
sbencke3
Associate II
Posted on May 17, 2011 at 11:53

I am trying to do the same thing, and I receive the same response. Did you resolve this problem ?

yu-jun
Associate II
Posted on May 17, 2011 at 11:53

In the PSDsoft Express there si a fuction: STMicroelectronics Conventional Programmers.

Run it, you should come into a dialog.

In the dialog you press the button --- Upload. the data in the uPSD can been load.

If the data is protected, you can't do it.
babidesai123
Associate II
Posted on May 17, 2011 at 11:53

just now i tried with that ..but it's showing the dialog box showing

''device upsd3234A is currently not supported under psd pro''

plz help
sjo
Associate II
Posted on May 17, 2011 at 11:53

If using the Flashlink do an upload in the JTAG/ISP section

Regards

sjo
sbencke3
Associate II
Posted on May 17, 2011 at 11:53

Ok, but in this section I can't read the device, can I?

jdaniel
Associate II
Posted on May 17, 2011 at 11:53

Yes, you can... in the ''Step 2'' section, the first box normal has ''Program/Verify'' selected or something of the like. Just change it to upload.