cancel
Showing results for 
Search instead for 
Did you mean: 

emulator with trace

tibo
Associate II
Posted on June 13, 2008 at 17:51

emulator with trace

2 REPLIES 2
tibo
Associate II
Posted on May 17, 2011 at 12:37

Hi ST1,

we are searching for a trace emulator for the stm32. I think Signum

has a good trace emulator with stm32 support (with ITM and ETM), but

it was very expensive for a ''low cost'' chip like stm32.

I found on the homepage of Signum an ARM Evaluation Kit ''JTAGjet-

Trace-STM''. The price is $2.500,- (normal price > $3.500,-). So I

asked Signum, if it can be used with stm32. Here is the answer:

> This was a special OEM version of JTAGjet-Trace which was

> designed for ST. ST commissioned Raisonance to supply a

> complete solution for STR9 including our JTAGjet-Trace. So we

> built them a special firmware inside to limit its operation to STR9

> devices only and sold it for $2,500.

>

> This item is only available from ST or its distributors.

Now my question to ST is, if it is possible to make this trace

emulator available for the stm32-community. I think it is only a

question of licensing and not of hardware/software, because Signum

supports already the stm32.

Thanks!

16-32micros
Associate III
Posted on May 17, 2011 at 12:37

Dear Tibo,

Thank for your detailed request. Me too I have an JTAGJetTrace working with STR9 but not yet for STM32 High-density devices that supports trace/ETM. I will note your point and check my colleagues if we can negociate with Signum to provide this service and a full package with STM32.

However I can suggest you to check with Segger in germany at www.segger.com :

http://www.segger.com/jtrace_general.html

(Less than 1000Euros) , I believe that they are already working on STM32.

I can also advice you to use Serial Wire Viewer for extreme low-cost solution but with limited features at :

http://www.st.com/mcu/contentid-115.html

Hope this is us useful for you :-)

Cheers,

STOne-32 ... Welcome to our recently 8-bit STM8S Family too :-)