cancel
Showing results for 
Search instead for 
Did you mean: 

New Lib v 3.0.0 don't support C++?

hemicuda
Associate II
Posted on May 27, 2009 at 02:56

New Lib v 3.0.0 don't support C++?

4 REPLIES 4
hemicuda
Associate II
Posted on May 17, 2011 at 13:12

In new Library v.3.0.0 startup file doesn't correctly works with cpp projects (IAR IDE) ?

''when any interrupt is generated, the pointer comes in asm interrupt implementation (startup_stm32f10x_xd.s) and remains there, and don't jump into my interrupt handler (stm32f10x_it.c)''

b239955_stm1_st
Associate
Posted on May 17, 2011 at 13:12

Try compiling with the option extension based. its due to name decoration when using c++

hemicuda
Associate II
Posted on May 17, 2011 at 13:12

Quote:

On 25-05-2009 at 10:22, Anonymous wrote:

Try compiling with the option extension based. its due to name decoration when using c++

I try this way, but it didn't works. Problem with the interrupts is still actual.

rael
Associate II
Posted on May 17, 2011 at 13:12

My problem is that I don't have a stm32f10x_it.c file in my project, or, as far as I can see included in any of the files used in it.

I can't find the vector table, or the interrupt handlers.

If I brouse to the pgmfiles\raisonance\ride\lib\arm\stm32f10x_lib\examples, I can find such files, but I can't see any #include directives to get my own one for the project, and yet I presume the main.c main routine is entered by a jump from a vector table reset address. I want to identify this clearly.. so I can get on with my project. :-o