2017-12-05 07:49 AM
hi,
in the UM2114 V2.0 for cmd AT+S.FSL and AT+SFSP there is a note:
Note that Volume ID 3, Application Flash, when protected (
app_fs
status variable set to 2) does not show content files.I don't see this variable nowhere!
How can i check this variable in the wifi module?
Yoann
Solved! Go to Solution.
2017-12-05 09:07 AM
Thank you Gerardo,
but AT+SSTS give nothing!
AT+S.STS
AT-S.ListAT-S.Var:nv_manuf=STMicroelectronics Inc.AT-S.Var:nv_model=SPWF04SAAT-S.Var:nv_serial=17111984AT-S.Var:nv_wifi_macaddr=00:80:E1:BD:00:71AT-S.Var:standby_time=10AT-S.Var:standby_enabled=0AT-S.Var:sleep_enabled=0AT-S.Var:etf_mode=0AT-S.Var:blink_led=1AT-S.Var:ext_volume=0AT-S.Var:ramdisk_memsize=16AT-S.Var:aes128_key=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:61AT-S.Var:user_desc=nonymousAT-S.Var:python_script=3:/uPython_test.pyAT-S.Var:python_memsize=32AT-S.Var:console_enabled=1AT-S.Var:console_speed=115200AT-S.Var:console_hwfc=0AT-S.Var:console_echo=1AT-S.Var:console_errs=2AT-S.Var:console_winds=2AT-S.Var:console_verbose=1AT-S.Var:console_repeater=0x21AT-S.Var:console_delimiter=0x2CAT-S.Var:console_wind_off_low=0x00000000AT-S.Var:console_wind_off_medium=0x00000000AT-S.Var:console_wind_off_high=0x00000000AT-S.Var:wifi_tx_msdu_lifetime=0AT-S.Var:wifi_rx_msdu_lifetime=0AT-S.Var:wifi_operational_mode=0x00000011AT-S.Var:wifi_beacon_wakeup=1AT-S.Var:wifi_beacon_interval=100AT-S.Var:wifi_listen_interval=0AT-S.Var:wifi_rts_threshold=3000AT-S.Var:wifi_ssid=6C:65:62:65:6C:6C:79:31:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00AT-S.Var:wifi_ssid_len=8AT-S.Var:wifi_txfail_thresh=5AT-S.Var:wifi_dtim_period=1AT-S.Var:wifi_add_tim_ie=0AT-S.Var:wifi_region=1AT-S.Var:wifi_ht_mode=1AT-S.Var:wifi_channelnum=11AT-S.Var:wifi_opr_rate_mask=0x003FFFCFAT-S.Var:wifi_bas_rate_mask=0x0000000FAT-S.Var:wifi_mode=1AT-S.Var:wifi_auth_type=0AT-S.Var:wifi_atim_window=0AT-S.Var:wifi_powersave=0AT-S.Var:wifi_tx_power=18AT-S.Var:wifi_rssi_thresh=0AT-S.Var:wifi_rssi_hyst=0AT-S.Var:wifi_ap_idle_timeout=120AT-S.Var:wifi_beacon_loss_thresh=10AT-S.Var:wifi_priv_mode=0AT-S.Var:wifi_wep_keys[0]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00AT-S.Var:wifi_wep_keys[1]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00AT-S.Var:wifi_wep_keys[2]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00AT-S.Var:wifi_wep_keys[3]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00AT-S.Var:wifi_wep_key_lens=00:00:00:00AT-S.Var:wifi_wep_default_key=0AT-S.Var:wifi_wpa_psk_raw=74:CF:1B:3F:23:69:3E:2E:1B:29:83:C6:75:42:8F:F3:6F:31:2C:AA:29:EB:E2:AB:87:F7:F9:83:8C:D0:98:19AT-S.Var:wifi_wpa_psk_text=SRRXTW6NAT-S.Var:wifi_eap_identity=identityAT-S.Var:
mailto:wifi_eap_anon_identity=anonymous@identity.org
AT-S.Var:wifi_eap_passwd=passwordAT-S.Var:wifi_eap_type=0AT-S.Var:wifi_eap_skip_datechecks=0AT-S.Var:wifi_wps_walk_time=120AT-S.Var:wifi_wps_pin=1234567AT-S.Var:ip_sock_memsize=1AT-S.Var:ip_sock_threshold=0AT-S.Var:ip_dhcp_lease_time=120AT-S.Var:ip_macfilter=00:00:00:00:00:00AT-S.Var:ip_num_clients=5AT-S.Var:ip_allow_port_scans=1AT-S.Var:ip_use_v6=1AT-S.Var:ip_use_dhcpd=1AT-S.Var:ip_use_httpd=1AT-S.Var:ip_use_tftpd=1AT-S.Var:ip_use_dhcpc=2AT-S.Var:ip_hostname=iwm-BD-00-71AT-S.Var:ip_apdomainname=captiveportal.netAT-S.Var:ip_apredirect=firstset.htmlAT-S.Var:ip_ipaddr=192.168.0.50AT-S.Var:ip_netmask=255.255.255.0AT-S.Var:ip_gw=192.168.0.1AT-S.Var:ip_dns1=208.67.222.222AT-S.Var:ip_dns2=208.67.220.220AT-S.Var:ip_local=0:0:0:0:0:0:0:0AT-S.Var:ip_dns1v6=0:0:0:0:0:0:0:0AT-S.Var:ip_dns2v6=0:0:0:0:0:0:0:0AT-S.Var:ip_dhcp_timeout=20AT-S.Var:ip_ntp_server1=ptbtime1.ptb.deAT-S.Var:ip_ntp_server2=ntp0.ipv6.fau.deAT-S.Var:ip_ntp_refresh=3600AT-S.Var:ip_ntp_startup=1AT-S.Var:ip_mdns_domain_name=SPWF04S-DefaultAT-S.Var:ip_mdns_device_name_ttl=120AT-S.Var:ip_mdns_services_name=SPWF04S-WebSrv SPWF04S-TFTPSrvAT-S.Var:ip_mdns_services_prot=_http._tcp _tftp._udpAT-S.Var:ip_mdns_services_keys=dev1 dev2AT-S.Var:ip_mdns_services_vals=number1 number2AT-S.Var:ip_mdns_services_port=80 69AT-S.Var:ip_mdns_services_ttl=120 60AT-S.Var:ip_mdns_startup=01:01AT+S.STS=app_fs give a result : AT-S.Var:app_fs=1.
and i just find explanation in the UM2114 V2.0 Table 9: Status variables!
thanks
Yoann
2017-12-05 07:56 AM
AT+S.STS (full list) or
AT+S.STS=app_fs (that variable)
2017-12-05 09:07 AM
Thank you Gerardo,
but AT+SSTS give nothing!
AT+S.STS
AT-S.ListAT-S.Var:nv_manuf=STMicroelectronics Inc.AT-S.Var:nv_model=SPWF04SAAT-S.Var:nv_serial=17111984AT-S.Var:nv_wifi_macaddr=00:80:E1:BD:00:71AT-S.Var:standby_time=10AT-S.Var:standby_enabled=0AT-S.Var:sleep_enabled=0AT-S.Var:etf_mode=0AT-S.Var:blink_led=1AT-S.Var:ext_volume=0AT-S.Var:ramdisk_memsize=16AT-S.Var:aes128_key=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:61AT-S.Var:user_desc=nonymousAT-S.Var:python_script=3:/uPython_test.pyAT-S.Var:python_memsize=32AT-S.Var:console_enabled=1AT-S.Var:console_speed=115200AT-S.Var:console_hwfc=0AT-S.Var:console_echo=1AT-S.Var:console_errs=2AT-S.Var:console_winds=2AT-S.Var:console_verbose=1AT-S.Var:console_repeater=0x21AT-S.Var:console_delimiter=0x2CAT-S.Var:console_wind_off_low=0x00000000AT-S.Var:console_wind_off_medium=0x00000000AT-S.Var:console_wind_off_high=0x00000000AT-S.Var:wifi_tx_msdu_lifetime=0AT-S.Var:wifi_rx_msdu_lifetime=0AT-S.Var:wifi_operational_mode=0x00000011AT-S.Var:wifi_beacon_wakeup=1AT-S.Var:wifi_beacon_interval=100AT-S.Var:wifi_listen_interval=0AT-S.Var:wifi_rts_threshold=3000AT-S.Var:wifi_ssid=6C:65:62:65:6C:6C:79:31:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00AT-S.Var:wifi_ssid_len=8AT-S.Var:wifi_txfail_thresh=5AT-S.Var:wifi_dtim_period=1AT-S.Var:wifi_add_tim_ie=0AT-S.Var:wifi_region=1AT-S.Var:wifi_ht_mode=1AT-S.Var:wifi_channelnum=11AT-S.Var:wifi_opr_rate_mask=0x003FFFCFAT-S.Var:wifi_bas_rate_mask=0x0000000FAT-S.Var:wifi_mode=1AT-S.Var:wifi_auth_type=0AT-S.Var:wifi_atim_window=0AT-S.Var:wifi_powersave=0AT-S.Var:wifi_tx_power=18AT-S.Var:wifi_rssi_thresh=0AT-S.Var:wifi_rssi_hyst=0AT-S.Var:wifi_ap_idle_timeout=120AT-S.Var:wifi_beacon_loss_thresh=10AT-S.Var:wifi_priv_mode=0AT-S.Var:wifi_wep_keys[0]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00AT-S.Var:wifi_wep_keys[1]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00AT-S.Var:wifi_wep_keys[2]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00AT-S.Var:wifi_wep_keys[3]=00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00AT-S.Var:wifi_wep_key_lens=00:00:00:00AT-S.Var:wifi_wep_default_key=0AT-S.Var:wifi_wpa_psk_raw=74:CF:1B:3F:23:69:3E:2E:1B:29:83:C6:75:42:8F:F3:6F:31:2C:AA:29:EB:E2:AB:87:F7:F9:83:8C:D0:98:19AT-S.Var:wifi_wpa_psk_text=SRRXTW6NAT-S.Var:wifi_eap_identity=identityAT-S.Var:
mailto:wifi_eap_anon_identity=anonymous@identity.org
AT-S.Var:wifi_eap_passwd=passwordAT-S.Var:wifi_eap_type=0AT-S.Var:wifi_eap_skip_datechecks=0AT-S.Var:wifi_wps_walk_time=120AT-S.Var:wifi_wps_pin=1234567AT-S.Var:ip_sock_memsize=1AT-S.Var:ip_sock_threshold=0AT-S.Var:ip_dhcp_lease_time=120AT-S.Var:ip_macfilter=00:00:00:00:00:00AT-S.Var:ip_num_clients=5AT-S.Var:ip_allow_port_scans=1AT-S.Var:ip_use_v6=1AT-S.Var:ip_use_dhcpd=1AT-S.Var:ip_use_httpd=1AT-S.Var:ip_use_tftpd=1AT-S.Var:ip_use_dhcpc=2AT-S.Var:ip_hostname=iwm-BD-00-71AT-S.Var:ip_apdomainname=captiveportal.netAT-S.Var:ip_apredirect=firstset.htmlAT-S.Var:ip_ipaddr=192.168.0.50AT-S.Var:ip_netmask=255.255.255.0AT-S.Var:ip_gw=192.168.0.1AT-S.Var:ip_dns1=208.67.222.222AT-S.Var:ip_dns2=208.67.220.220AT-S.Var:ip_local=0:0:0:0:0:0:0:0AT-S.Var:ip_dns1v6=0:0:0:0:0:0:0:0AT-S.Var:ip_dns2v6=0:0:0:0:0:0:0:0AT-S.Var:ip_dhcp_timeout=20AT-S.Var:ip_ntp_server1=ptbtime1.ptb.deAT-S.Var:ip_ntp_server2=ntp0.ipv6.fau.deAT-S.Var:ip_ntp_refresh=3600AT-S.Var:ip_ntp_startup=1AT-S.Var:ip_mdns_domain_name=SPWF04S-DefaultAT-S.Var:ip_mdns_device_name_ttl=120AT-S.Var:ip_mdns_services_name=SPWF04S-WebSrv SPWF04S-TFTPSrvAT-S.Var:ip_mdns_services_prot=_http._tcp _tftp._udpAT-S.Var:ip_mdns_services_keys=dev1 dev2AT-S.Var:ip_mdns_services_vals=number1 number2AT-S.Var:ip_mdns_services_port=80 69AT-S.Var:ip_mdns_services_ttl=120 60AT-S.Var:ip_mdns_startup=01:01AT+S.STS=app_fs give a result : AT-S.Var:app_fs=1.
and i just find explanation in the UM2114 V2.0 Table 9: Status variables!
thanks
Yoann
2017-12-05 09:13 AM
Full list you wrote is the output of AT+S.GCFG, and not AT+S.STS
2017-12-05 09:26 AM
i confirm i use cmd AT+S.STS.
it's include at the beginning of the copy/pass in the previous message (AT+S.STS)!
Yoann
2017-12-06 01:08 AM
hi,
i reloaded FW1.1.0 and AT+SSTS give good response now 'status variables'.
Something bad before...Mea culpoa ;-)
AT+S.STS
AT-S.ListAT-S.Var:build=171117-0328fe3-SPWF04SAT-S.Var:fw_version=1.1.0AT-S.Var:boot_version=1.0AT-S.Var:var_version=2...AT-S.Var:app_fs=1AT-S.Var:ram_fs=1AT-S.Var:user_fs=0AT-S.Var:extvol_fs=0...AT-S.OK