SPI Receive problem
Hi all,
I am trying to read a four bytes register from TDC-GP30 ultrasonic flow converter using HAL_SPI_Receive function. Below is the code that I am using for reading the register contents:
/*******************************************************************************
* Function Name: gp30_read_n_bytes * Parameters: n_bytes = how many bytes should be read * read_opcode = read opcode of the device * read_addr = read address of the device * * Return: n bytes from the specified read address * * Description: Reads n bytes from an address in GP30 * ******************************************************************************/float gp30_read_4_bytes(uint8_t read_opcode, uint8_t read_addr){ uint32_t Result_read = 0x00000000; uint8_t Result_read_buff = 0x00; GP30_SPI_enable(); HAL_SPI_Transmit(&hspi1,&read_opcode,1,100); HAL_SPI_Transmit(&hspi1,&read_addr,1,100); HAL_SPI_Receive(&hspi1,&Result_read_buff,1,100); Result_read |= (Result_read_buff<<24); HAL_SPI_Receive(&hspi1,&Result_read_buff,1,100); Result_read |= (Result_read_buff<<16); HAL_SPI_Receive(&hspi1,&Result_read_buff,1,100); Result_read |= (Result_read_buff<<8); HAL_SPI_Receive(&hspi1,&Result_read_buff,1,100); Result_read |= (Result_read_buff); GP30_SPI_disable(); return Result_read;}The problem is that I cannot receive all four bytes. For example one register contains 0x12345678 and when I read its content I receive 0x12345600 all the time. Its receiving fine for some other values but not for all values.