Read our guidelines, share your thoughts about your community experience, and explore community insights.
Most recent activity
Neither in the front page listing, nor in the individual forums. New threads used to be highlighted in bold on the old forum.
Example: Could be because it is a start post. But I find it useful to be able to quote specific parts of a start post and reply to those specific parts.
The following items were not carried overIt seems that Following & Followers were also not carried over ?(not that I’m concerned by this - just an observation)
Just for fun...i tried to use the SPI on H743 by direct setting and writing to registers:- i never got it working on some attempts years ago, so just used HAL , which just works.- now i tried again: cannot be, its so difficult...- ok, its a over complicated construction....old SPI on F303 works instantly and fast, no problem there.- but now have AI ... can it help?So i tried Sidekick, it should be easy for him...it...whatever...I asked how to do...in German, more easy for me - and a test: can it understand...?Sidekick tells:3. ZusammenfassungUm auf dem STM32H743 einen SPI-Transfer durch Schreiben auf SPI_TXDR zu starten, müssen Sie:Die Datenlänge im SPI_CFG1-Register korrekt einstellen,die Bitreihenfolge im SPI_CFG2-Register wählen,die relevanten GPIOs konfigurieren,das SPI-Modul aktivieren,und dann die Daten in der konfigurierten Länge auf SPI_TXDR schreiben.Ein Schreibzugriff mit weniger als der konfigurierten Datenlänge ist nicht zulässig.--- THIS didnt help me, as it also just brin
Wasn't anywhere near ST site but got this email:Please click on this button to start the download of the requested content:${ctatext}Was this a test gone wrong? Did anyone else get it? Do I need to contact support?Just posting here in case anyone else got it.
Hello,would like to change the email address on my ST Community account. I cannot find the option in the settings. Could an admin assist with updating my email? Thank you!
2026年,1月30日,STM32 Sidekick看不到了。出故障了吗? Google translation: On January 30, 2026, the STM32 Sidekick was no longer visible. Was it malfunctioning? Please note that the language of the forum is English - see the Terms & Conditions.
I get this error when I press the 'Kudos' button: https://community.st.com/t5/stm32-mcus-products/stm32g411-availability/m-p/885372/highlight/true#M293512 Also happens on other posts in that thread, and in other threads. Looks like a recurrence of Kudos button gives error (12 Dec 2025)
Had a few of these these morning
I've seen it a couple of times - both from ST Employees, IIRC; eg,https://community.st.com/t5/mems-sensors/lsm6dso-and-lsm6dso32-compatible/m-p/891941/highlight/true#M27029 Neither the button nor the option allows just formatting a single word like that. Looking at the HTML view of the above post, it's using the <code> tag - but I don't see any way to enter that via the Editor?(I did that one via the HTML editor - but that's very klunky!)
Tried to paste code in reply. Noticed, that line count does not match. Clicked in editor and it started to duplicate.Also check out attached video.In order to reproduce the bug, longer code must be pasted in C code insert tool from tool bar. Then mouse pointer must be navigated at the end of inserted code and clicked few times here and there. Inserted code will start to duplicate in editor.
For the past week or so, pasting images directly into posts seems to have broken.I used to be able to just take a screenshot, or copy an image and paste it straight into the editor, but that no longer works.I press 'paste', and nothing happens - no error messages or anything.I am now having to save the image locally, and then use the 'Insert Photos' button to import it. There is history with this, but now it seems to have just broken completely. Using Chrome Version 145.0.7632.109 (Official Build) (64-bit) on Windows-11 Pro
Between Last Day to Last Year, doesn't show users. Only All Time shows users.
144 characters
Or 'Feature Request' or similar.Applies to CubeIDE, CubeMX, and CubeMX2 - probably also others ...eg, see here and here.
My post was deleted without any notification or reason? https://community.st.com/t5/escalated-topic/stm32h5-fdcan-system-bootloader/m-p/886189#M30060
so it seems:https://community.st.com/t5/stm32-mcus-embedded-software/sd-card-no-file-system-error/m-p/641421/highlight/true#M45513On other forums, the 'Mark As Solution' just changes to 'Unmark Solution' (or whatever) - so it's always obvious, and in the same place. Addendum:Perhaps this: https://community.st.com/t5/stm32-mcus-embedded-software/sd-card-no-file-system-error/m-p/641422/highlight/true#M45514 could be added here: https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256
Currently, questions are going in the Interface and connectivity ICs forum, but there don't seem to be any suitable labels:I don't think 'Low Power RF Solutions' really covers it?The Product Page on the main website comes under 'Wireless connectivity > Long range > NB-IoT products':So I guess that would be a good set of labels?
I'm trying to reply to a post. I'm logged in. I typed a response and attached an image with the "Insert Photos" tool. After hitting Reply, I see the message "An Unexpected Error has occurred". I've seen this a few times over the past week but didn't both posting this bug report until now.Anyone else?
When writing a reply, if the message includes images, parts of the post can be deleted after pressing the "Reply" button. This has happened many times over the last week. Since the data is deleted, there is no way to recover but to edit and re-enter that information.This is a big waste of time. Why is the forum software getting worse?
Since ~2 hours I get thousands of mails from notification@communitymailer.st.com mainly with STM8 stuff from the last years.What's going wrong here? Is it only me? I never was interested in STM8, just STM32...(I unsubscribed from "others: hardware and software" to survive the day.) P.S.: they all have the same init line like this:Hi mfgkw, Lina_DABASINSKAITE (Community manager) moved a topic in Others: hardware and software on 2020-09-08 8:15 AM: Where can I get the stm8s discovery dev.zip file? I would like to download the application code that is advertised with the eval/demo board but can't find it anywhere on ST.com. Thanks. They all seem to start with "Lina_DABASINSKAITE (Community manager) moved a topic in Others: hardware and software on " ...
See:User authentication service maintenance on 26 February (CubeIDE forum);User authentication service maintenance on 26 February (CubeMX forum).Neither of these says what time the maintenance is scheduled to occur. Temporary Unavailability of Server Update Pack – Maintenance on February 26 (in the VSCode forum) does give a time, but no timezone.
On some post now I get an errorHave been on this forum for 8 years or so, never had this issue..I tried to report a fix to someone, can't do that.. This is a great way to block uses reporting solutions.What is this ? Cannot find any link how to verify.Please help ASAPI also don't see Sidekick on any forum, is that related ?
In all the areas which currently have labels for the other peripherals. See: STM32H5E4/E5/F4/F5 with PLAY: boards availability?.
The current marking is one character per line and it bleeds into other posts. Looks very amateur. The new forum has been here for many years at this point, can we improve the presentation here?
ST Community highlights – April to June 2026
Already have an account? Login
No account yet? Create an account
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.