Skip to main content
CTapp.1
Senior III
Jun 12, 2026 10:26 AM UTC
Question

No new lines in signatures

It isn’t possible to add new lines in signatures.

8 replies

Andrew Neil
Super User
Jun 12, 2026 10:46 AM UTC

(never mind)

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
CTapp.1
CTapp.1Author
Senior III
Jun 12, 2026 11:25 AM UTC

Just noticed that my signature now seems to not be showing at all.

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
CTapp.1
CTapp.1Author
Senior III
Jun 12, 2026 11:26 AM UTC

But it does in replies!

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
Lina_DABASINSKAITE
ST Community Manager
Jun 12, 2026 12:55 PM UTC

Hello ​@CTapp.1,


The out-of-the-box setting is to embed plain text. The signature component does not support HTML, so line breaks cannot be introduced in this way.

As ​@Andrew Neil  mentioned, line breaks occur naturally because of page wrapping.

The signature should appear only in replies. This behavior was also present on the previous platform.

Kind regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
CTapp.1
CTapp.1Author
Senior III
Jun 12, 2026 1:11 PM UTC

I don’t think I used HTML to create them previously - just the edit box allowed carriage returns to be entered.

I use a multi-line signature so that I can add a disclaimer and acknowledge my affiliations to ensure there is no undeclared conflict of interest or an implied implication that I am posting in an official capacity. Something like:

All posts are made in a personal capacity
MISRA C++ Chair
MISRA C WG Member
Director The MISRA Consortium Limited (TMCL)

Not a great loss if I have to change that into a single line, but it won’t be so easy to read 😉

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
Lina_DABASINSKAITE
ST Community Manager
Jun 12, 2026 1:23 PM UTC

​@CTapp.1 , I checked and yes the previous signature box was a bit more flexible than this one. 
 

Perhaps you can use some symbols, such as | to make more structured or anything else :) 

Kind regards,
Lina

 

 

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.