Skip to main content
Andrew Neil
Super User
Jun 9, 2026 2:47 PM UTC
Question

Need a 'Mark All As Read' option

There was one in the old forum.

Having to visit every single thread individually - especially the ones in which I have no interest and nothing to contribute - just to get rid of the ‘New’ highlighting is going to be a real pain!

2 replies

Andrew Neil
Super User
Jun 10, 2026 11:27 AM UTC

The ‘Notifications’ list has it:

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Lina_DABASINSKAITE
ST Community Manager
Jun 11, 2026 1:46 PM UTC

Hi ​@Andrew Neil,

Thanks for sharing this.

I understand this is causing inconvenience at this moment but not all previously available features are available on this platform.

I am checking if there is anything on roadmap for this. 
 

Feedback from other users is also welcome to help assess the feature's importance.

Kind regards,
Lina

 

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.