Skip to main content
unsigned_char_array
Lead III
Jun 9, 2026 11:22 AM UTC
Question

New community platform: quoting some posts not possible

Example:

 

Could be because it is a start post. But I find it useful to be able to quote specific parts of a start post and reply to those specific parts.

2 replies

Lina_DABASINSKAITE
ST Community Manager
Jun 9, 2026 1:53 PM UTC

Hi ​@unsigned_char_array , 
 

Thank you for bringing this up. It can be done by selecting the Quote button in the editor, and then clicking Insert paragraph here.

 


This action splits the quote and adds space for the text. Quotes and text can then be added as needed. Example below:

 


Your text 1

 Could be because it is a start post. But I find it useful to be able to quote specific parts of a start post and reply to those specific parts.

 
Your text 2
 

 Could be because it is a start post. But I find it useful to be able to quote specific parts of a start post and reply to those specific parts.

 

Test it and let me know how it works.

Thanks,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
unsigned_char_array
Lead III
Jun 9, 2026 2:12 PM UTC

The quote button in the reply editor just adds an empty quote. Of course you could manually copy texts and images from the post, but that is extra work. It also leaves out the author name. Though that is kind of obvious.
Adding a quote using the tripple dot menu and deleting the unused parts of the quotes can be quicker.

 

In addition the quote button doesn’t quote a code block properly. There is no syntax highlighting, it’s all red. The previous forum platform also had issues with quoting posts with code.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."