2017-05-16 1:15 PM
Hi, I am using the
SPC570S40E1 microcontroller. When looking at the MOSI line on the scope, I am seeing spikes right around the end of a frame even when transmitting all zeros. The device I am trying to communicate with requires a 40 bit message. To achieve that, I am sending 16,16 and 8 bit frames.
There is one spike at beginning of the second frame and another at the beginning of the third frame.
Also, regarding the Fast Continuous PC mode, which allows masking the Tasc and Tcsc delays, is there a way to enable the masking of delays without also enabling parity bit transmission.
Thanks
Update: I don't see any spikes if I enable continuous clock, but I am still looking for a solution without having to do that. I tried lowering the baud rate and adjusting the delays( Tasc and Tcsc), but that didn't work.
#spi2017-05-17 7:10 AM
Hello ,
After checking with experts, I think that it is not possible
The delays can be masked in Fast Continuous PC mode
1 Fast Continuous PCS mode. Delays masked via control bits in PUSHR.
cf bit PE_MASC
Parity Enable or Mask tASC delay in the current frame PE
This bit enables parity bit transmission and parity reception check for the SPI frame.
Best regards
Erwan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.