cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMx 4.20.1: Clock Configuration GUI not working

Katzenberger.Michael
Associate III
Posted on April 21, 2017 at 20:49

Hi all!

The Clock Configuration GUI shows a weird behavior: I'm not able to put a valid input frequency for HSE (or LSE).

For example I want to setup the input frequency to 8 MHz:

  • entered value 8 is not accepted - changed to 0.0000000000080 immediately0690X00000606ogQAA.png
  • entered value 8000000 is accepted and changed to value 8 but as soon as the focus is changed to an other element the value jumps to 0.0000080 0690X00000606qCQAQ.png

Development environment:

  • Eclipse Neon 3
  • STM32CubeMx version: 4.20.1 (Eclipse plugin)
  • Java: jdk1.8.0_25
  • ioc config file attached

Best regards,

Michael.

This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9
Katzenberger.Michael
Associate III
Posted on April 21, 2017 at 21:27

short test: downgrading version until GUI is working

STM32CubeMx version

GUI is working

4.20.1

:)

4.20.0

:)

4.19.0

:)

4.18.0

Khouloud GARSI
Lead II
Posted on April 27, 2017 at 12:47

Hi

Katzenberger.Michael

‌,

I'm not able to reproduce your issue.

Could you please create a new project using CubeMX V4.1 and check if the issue persist.

Khouloud.

Posted on April 27, 2017 at 21:56

Hi Khouloud,

I've reinstalled version V4.20.1 and can confirm that the problem still exists

create new project

0690X000006062oQAA.png

enable High Speed Clock

0690X00000606t1QAA.png

Default clock setting shown good as expected

0690X00000606tLQAQ.png

but as soon I change the default value the GUI shows wrong values

0690X00000606tHQAQ.png

clock values entered in Hz (e.g. 10000000) are temporarily accepted as 10 MHz but as soon as I change the focus (activate another element) the entered value becomes invalid.

Same for my Nucleo STM32F411RE ...

Sirma Siang
ST Employee
Posted on May 03, 2017 at 10:12

Hello katzenberger.michael,

I would like to thank you for your feedback, and indeed, such behaviour has been observed using eclipse plugin.

This does not happen using CubeMX in standalone mode.

We are looking why cube comportment is different when launching from Eclipse.

KR

Sirma
Posted on August 11, 2017 at 10:25

Hello, I have exactly same experiences. In actual version of Eclipse plug-in (4.22.0) still nothing has changed to better. Please, will it ever be resolved ?

Thanks and have a nice day,

Peter

Posted on August 21, 2017 at 16:27

Hello

kovar.petr

,

We are currently redesigning CubeMX integration into Eclipse. As this is a significant amount of work, it is quite difficult to give an availability date right now.

Kind regards

Sirma

Posted on February 21, 2018 at 23:43

In version 4.24.0 this issue is still not solved. Is there not date yet defined to be resolved?

Posted on February 22, 2018 at 02:23

Try 

https://en.wikipedia.org/wiki/Reverse_psychology

 . Show them that you're not affected, that you don't care, praise those issues

:)

 
atomassini
Associate II
Posted on March 27, 2018 at 12:42

Hello, had the same issue but found a workaround:

the gui erroneously validates the frequency input dividing it by 100000 and rewriting the divided value to the textbox: this is the bug.

So,

you don't have to press enter

once the crystal frequency is entered (in Hz) into the textbox, but

simply move the focus to another component on the page (a prescaler combo, a radio button, whatever else).

Regards.