CubeMx dma spi:Getting spi overrun
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-01-24 5:39 AM
Hi,
I'm using latest version of Cube (download 20.01). I'm trying to read ADC-values from SPI with DMA. Read is activated on ADC-dataready.
#define ADC_BLOCK_SIZE 24
uint8_t tempBuf[ADC_BLOCK_SIZE ];
// This interrupt is called every 100 us.
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
status = HAL_SPI_Receive_DMA(&hspi1, tempBuf, ADC_BLOCK_SIZE);
}First read calls the DMA ready Callback correctly
HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
but further interrupts cause SPI overrun error and transfer stops. Any ideas what to do differently?
APB2 is at 42 MHz
I tested the same transfer with SPI polling method and it was working without errors.
/* SPI1 init function */
static void MX_SPI1_Init(void){hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init.Direction = SPI_DIRECTION_2LINES_RXONLY; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLE; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi1.Init.CRCPolynomial = 10; if (HAL_SPI_Init(&hspi1) != HAL_OK) { Error_Handler(); }}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-01-24 6:17 AM
Edit: i commented hal errorcode line, so code doesn't abort. Code running ok and the spi input values seems to be ok too.
I'm not really undestand what happening here. I have to test this more
/* SPI in Error Treatment --------------------------------------------------*/
if(((itflag & (SPI_FLAG_MODF | SPI_FLAG_OVR | SPI_FLAG_FRE)) != RESET) && ((itsource & SPI_IT_ERR) != RESET)) { /* SPI Overrun error interrupt occurred ----------------------------------*/ if((itflag & SPI_FLAG_OVR) != RESET) { if(hspi->State != HAL_SPI_STATE_BUSY_TX) { //SET_BIT(hspi->ErrorCode, HAL_SPI_ERROR_OVR); // Do not set error code __HAL_SPI_CLEAR_OVRFLAG(hspi); }