2017-04-29 6:37 AM
To prove a bad thing can get worse, I stitched together some of the HAL example code
This project takes RGB8888 bitmaps [max of 25] and uploads them to the QSPI Flash on-board. It outputs information on uart 1
https://github.com/ProjectsByJRP/uSDcard_to_QSPI_flash
This project takes the bitmaps in the QSPI flash and displays them on the on-board LCD. output on uart1