cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK CLI (v3) cannot connect with LPM option

nvkokorin
Associate II
Posted on September 14, 2017 at 11:02

Hi everybody!

Just I want read a some memory area from my F4-DISCO for monitoring values.

So, first I start 

ST-LINK CLI with following arguments:

ST-LINK_CLI.exe -c SWD HOTPLUG -r8 0x20018000 0x100

and this works (i.e. read data) fine, but processor gets the stop-state during data read and runs again after.

Second, I trying to run CLI with additional LPM option, like this:

ST-LINK_CLI.exe -c SWD HOTPLUG LPM -r8 0x20018000 0x100

But the ST-LINK CLI returns a error:

[LPM]: Unknown debug protocol or option!

I tried a different options and it different order in command line, but not success.

Who can explain what's going on with CLI and how I can resolve this issue?

Thanks!

#lpm #st-link-cli
This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9
nvkokorin
Associate II
Posted on October 10, 2017 at 08:51

hey developers! Is anyone here?

Martin Taylor
Associate II
Posted on June 28, 2018 at 17:04

Did you ever get a solution to this? The manual still says '-c LPM' is a valid option. I'm trying it today and getting the same error you got.

Posted on June 28, 2018 at 18:06

Hello 

mtaylor

 

Which version of STLink Utility is used ?

Can you please check if you use the latest version 4.2.0!

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on June 28, 2018 at 18:55

STM32 ST-LINK CLI v3.0.0.0

On Thu, Jun 28, 2018 at 12:07 PM, Imen D <st-microelectronics@jiveon.com>

________________

Attachments :

image.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxSd&d=%2Fa%2F0X0000000ayK%2FdHByI7M3t2yam_QqxMTneCiqC3CTEkq6ybr4B80FLx0&asPdf=false
Posted on June 28, 2018 at 19:21

Upgrading to 4.2.0/3.2.0.0.0 made the LPM option work OK.

On Thu, Jun 28, 2018 at 12:08 PM, Imen D <st-microelectronics@jiveon.com>

Posted on June 28, 2018 at 20:29

Correction: No difference with 4.2.0/3.2.0.0.0. Still get the original

error with LPM option AND it screws up the ST-Linkj so bad you have to

unplug and replug the IF to get it to work again!

Posted on June 28, 2018 at 22:26

STLink Utility v.4.2 (with cli v.3.2) does not work also. The LPM option is not supported.

This was checked immediately as latest version has been released!

Posted on June 29, 2018 at 11:07

Hello 

K.N

 ,

Thank you for posting your update.

We will check this internally and come back to you.

with Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Imen.D
ST Employee

Hello,

This issue will be fixed with the next version of STM32 ST-LINK Utility (V4.3.0).

Kind Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen