cancel
Showing results for 
Search instead for 
Did you mean: 

Could you kindly fix the BUG in the SD card CubeMx v4.21.0

JMJV
Associate II
Posted on November 14, 2017 at 12:28

Hello ST team

I'm writing to you because I'm working on

STM32F746ZGTx, but I have found the same BUG problem with the SD card in CubeMx version 4.23.0 library Firmware package STM32F7 v1.8.0.

Before I was working with CubeMX 4.21.0 and Firmware Package 1.7.0  and the problem with the SD card was solved, now I updated with the new version 4.23.0 and seems the .h and .c files have a lot of changes (for instance the 

stm32f7xx_hal_sd.c file

)

Please, could you fix the issues?

best 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Amel NASRI
ST Employee
Posted on November 14, 2017 at 14:53

Hi

jacinto.juan

‌,

This should be the same issue as reported in

https://community.st.com/0D50X00009XkXvgSAF

.

We are already aware of this issue that should be fixed in next release.

Sorry for such inconvenience.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Amel NASRI
ST Employee
Posted on December 07, 2017 at 11:15

Hello,

Please refer to the following if you have similar issue:

-

https://community.st.com/0D50X00009bMM8bSAG

-

https://community.st.com/0D50X00009XkXg5SAF

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Jeanne Joly
Senior III
Posted on February 15, 2018 at 11:00

Hi

Jacinto.Juan

,

If you are talking about the issue highlighted here

https://community.st.com/0D50X00009bMM8bSAG

, indeed, the correction is available in the current CubeMX release (4.24).

Please, update your release with the latest one.

BR. Jeanne