A blanked flash STM32 was soldered on the PCB ?If yes, the chip is in bootloader mode.Do you see the oscillators running ?Do you see noise on the MCU Vdd ?Replace the Vdd to Vdda inductance by a 0 Ohm resistor. (increase the value if you need filteri...
The spec says the slave address is 0x60 (8 bit). Sometime functions require only 7 bits, so 0x30.the slave use a 8 bit sub address. at location 0x2F you can read the chip ID which is expected to be 0x0CYou should exit the loop only when the device is...
Posted on April 05, 2018 at 18:52https://www.digikey.com/products/en?keywords=p-l496g-cell01 113.75 USD, in stockDistributor's price.Thousands kits are being produced by ST to keep up with pending orders as we are in ramp up phase.Monitoring Q2 back...
Posted on February 15, 2018 at 20:13Availability at distributors planned early Q2, then shop around to get the best deal.Both CELL01 and CELL02 Discovery Packs will come at the same price.More details will be disclosed in March. Stay tuned!