Posted on May 17, 2011 at 09:59Hi all, Can TFT be interfaced with EMI of STR9? I want to interface WF57ETIBCDC# with display controller SSD1963 in 8bit mode. Thanks & Regards, Chandrakant.
Posted on May 17, 2011 at 09:59Hi, This problem is solved. I have replaced the MEMCOPY_L2S_BY4 (memcopy.s) by memcpy (string.h) & removed memcopy.s from project.
Posted on May 17, 2011 at 09:59Hi, I'am using STR9 Starter kit from IAR. When i try to build webserver demo. But i got following error while linking.''Error[Lp011]: section placement failed: unable to place sections/blocks with a total estimated min...
Posted on May 17, 2011 at 09:58I'm using STR912FA44 for our project. i'm not able to use RTC's periodic interrupt. when it is enabled CPU gets reset. Pls can anybody help me? my initialization routine is as follows: void InitRTC (Int32U IntrPriority...