User Activity

Hello everyone,We are currently trying to experiment with the STM32WB5M for it to be integrated in our project as a radio co-processor module.We have ported nimble stack (https://github.com/apache/mynewt-nimble) on our application MCU to act as an ho...
Hi,We are currently using an stm32l5 in our product and experimenting with a stm32L562E-dk and with the official TFM (https://git.trustedfirmware.org/TF-M/trusted-firmware-m.git master branch on the latest commit at this date.) The TFM is unmodified...
Hello,Our team is currently working on stm32mp1 boards (the dk2 and the ev1).Our software architecture is using TFA, OPTEE, Uboot and Linux.For our needs, we have developed an SPI driver for OPTEE. The OPTEE version on which we developed this driver ...
Hi,We are currently developing on the STM32MP1. Our goal now is to be able to debug the core at the different running stages : TF-A, Optee, U-boot and kernel. We are using the DK2 with a ST-link and openOCD.When using your Setup.gdb we experience som...
Hi,We are currently using the STM32MP1 DK2 board for our project.We have to use FreeRTOS + UART7 and USART3 with DMA Our issue arise when FreeRTOS is used with an UART (USART3 or UART7 in our case) which use the DMA.We have reduced the project to the...
Kudos from