User Activity

Hello,I am trying to get my ADC using DMA working in my freertos program running on the M33 core of the stm32mp257 processor. I set up ADC1 on HPDMA3 using cube MX see config below.I am getting a few issues.1. If I used the generated code I get a run...
Hello, I am trying to load an .elf file on the M33 core on my stm32mp257f processor. When I launch the remote core using remoteproc I get the following errors.       root@stm32mp257f-hydra-mx:~# echo -n /home/root > /sys/module/firmware_class/paramet...
Where can I find the STM32MP25_CM33.svd file?
Hello,I have a custom board with the STM32MP257FAK processor. I am having issues booting into u-boot from emmc. I can boot into u-boot fine using dfu-util over usb. But once I program in fsbl, ssbl, and meta data into the emmc and try to boot from it...
Hello,I have compiled a custom image to run on the M4 core on my stm32mp157f-dk2. I generated the code using STM32CubeMX. I am able to build it fine but am having issues launching it on the m4 core. Here are the commands that I run. echo executable.e...
Kudos from