User Activity

Hi,I have an issue with low power operation when using the USBPD library. We have successfully implemented a low power feature for our new product. After that we have started the development of a USBPD feature. The problem is, that after the function...
Hi,i am developing an embedded software based on the TCP Client example for CubeMX. During tests with large number of packets I have got an hard fault error. It seems that it happens on a re-transmit. The hard fault can be easy reproduced with origin...
Hello,I have done a big mistake. I was testing a provisioning using the system bootloader. For that I have changed the provisioning batch files. As a result I have set the product state to closed, before the keys where loaded.  Now I can not connect ...
Hi all,we are developing a product with the STM32H573. The idea is to use the STiRoT for secure firmware update. The MCU is connected to a Linux CPU via SPI. Now we plan to do the provisioning during the production using the Linux CPU that has a ethr...