Hello @potato_2,
Did you have a look into the following wiki article : Trace and debug scenario - UART issue ?
I would focus on chapter 3.
BR,
Christophe
Hello @jasonj2,
I will try to summarize :
- The SAI configuration looks good
- The Codec configuration looks good
- Several probe_defer because SAI doesn't seem to provide MCLK, but after a while, it seems to be there.
For me, we need to know if...
Hello @take_4,
To change Dropbear SSH port from 22 to 10022, you need to update the following file : /lib/systemd/system/dropbear.socket:
-ListenStream=22+ListenStream=10022
This file is also available as a symbolic link in etc folder: /etc/syst...
Hi @FarukSozuer,
Feel free to look into the wiki : see STM32CubeProgrammer flashlayout page : the size of metadata partition is 256kiB.
The STM32CubeProgrammer page could help you as well.
BR,
Christophe
Hi @FarukSozuer,
I think it does this because it cannot find the FWU_MDATA files.
You almost answered to your question : if tf-a can't find both metadata partitions, it generates a panic.
The MPU Ecosystem supports A/B mechanism by default, so...