The X-CUBE-MCSDK standard code works well at frequencies lower than 10kHz. The lowest supported PWM frequency is in fact 2kHz. The optimal PWM frequency depends on the motor parameters.
Yes, the smaller pin with smaller hole should be the gate. With the flat surface facing down and the gate pin oriented towards you, the pin on the right of gate pin is A while the left pin is K. This info is missing in the DS0642 - Rev 6 of the devic...
Going by the specs, it is an application specific board with size constrains designed for Drones with battery packs up to 6S LiPO. Higher rated components (especially capacitors) would have increased the form factor/cost of the design. For higher vol...
Going by the listed specs and size, the board indeed seems to be designed specifically for RC Drone applications powered by up to 6S LiPo battery packs.The form factor required for these applications may be hard to meet with higher voltage rated capa...
Hello Javierio,I recently used these boards to run a 110V DC motor in sensorless FOC. Works fine in my case. Can you please share the exact problem you are facing? Initially with my particular motor, the system was going into Overcurrent Protection (...