Hi,I am using AIS2IH.I can see in terminal window of my computerthat registers of data and temperature are zero's. 0 0 0 ...My program use the setup: ais2ih_cs_mode_set(&dev_ctx, AIS2IH_PULL_UP_DISCONNECT);ais2ih_i2c_interface_set(&dev_ctx, AI...
And the setup program is here:ais2ih_device_id_get(&dev_ctx, &whoamI);platform_delay(0x06333333);ais2ih_device_id_get(&dev_ctx, &whoamI);platform_delay(0x06333333);ais2ih_device_id_get(&dev_ctx, &whoamI);platform_delay(0x06333333);/* Restore default ...
Hi Federica!What is the setup?Hardware(schematic diagram?) or software() or timing diagram of the setup?void ais2ih_init(void){/* Initialize mems driver interface. */stmdev_ctx_t dev_ctx;ais2ih_reg_t int_route;dev_ctx.write_reg = platform_write;dev_...