User Activity

Hello, I developed a custom board with a pinmap based on stm32mp157f - dk2.I think if you match the pinmap and use the start package, lcd and other features will work.I re-created the sd card according to that advice, and I also rebooted it, but the ...
The first logo appears, but the display behind it does not work. Looking at the error message below, it seems like there is a problem with ext4. How can I solve it? Or did something go wrong?  NOTICE: CPU: STM32MP157FAC Rev.ZNOTICE: Model: STMicroele...
NOTICE: CPU: STM32MP157FAC Rev.ZNOTICE: Model: STMicroelectronics STM32MP157F-DK2 Discovery BoardINFO: PMIC version = 0x21INFO: Reset reason (0x14):INFO: Pad Reset from NRSTINFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000INFO: ...
We made a new board with STM32MP157FAC1.I tried booting with SD card with STM32MP1 Starter Package image of STM32MP157x-EV1.I am inquiring about the following error. NOTICE: CPU: STM32MP157FAC Rev.ZNOTICE: Model: STMicroelectronics STM32MP157F eval d...
I developed a new stm32mp157 board. Do I need to update the firmware to run A7 on stm32mp157? Or is the firmware already updated?