Hi,I don't think you will be able to log the raw CSI input signals using the Raspberry Pi, or with a logic analyzer. You would need a scope with a MIPI CSI analyzer, which should work fine. We are compliant with the MIPI interface.To ensure the exact...
Hi,Good to know that it is working!UI stand for User Interface, which denotes a type of memory accessible to the host. So yes, it is the same registers that you can change with the EVK GS software and described in the user manual. The code examples t...
Hi Aster,Sure. I am not certain that we can read the metadata from PNG images, or at least not without a specific tool. You can also save the images as PGM files and use Notepad to read the metadata easily.Regards, Megane
Hello,The procedure seems good. Indeed, our drivers have been updated to work on RPI 5.To facilitate debugging, could you please reboot the board and share the log generated by the dmesg command? This will help us determine whether the issue originat...
Hello,Yes, the camera board is fully compatible with the Raspberry Pi as mentioned in the documentation. Indeed, the reset is controlled by the GPIO. Regarding the swapped pins you mentioned, it will be fine if you simply swap the flex cable; it shou...