Update: I heard back from ST support, it was a bug in their software, the bug is now resolved in a newer version of the Cube Programmer (v2.18). I tested it and it works as intended :)
RGari,I got that hint from a ticket, but I'm still waiting for further explanations and instructions. Also will post here as soon as I learn something usefull.Just to clarify, my DA auth is a success (based on CLI output) but the chip still remains i...
Hi, I observed the same issue on the same chip:The parsing error seems to go away if you change the header to match the password lenght and remove the 8.I changed 0x00 00 00 80 0C 00 00 00 (default password lenght is 0x0c) to 0x00 00 00 00 0F 00 00 0...
Hi,I did try that script with no luck, just bricks the chip every time.I have opened a support ticket and will continue there, thank you! If and when I have the solution I will follow up here to help others with the same problem. Regards,Mataj Zandon...