Posted on May 17, 2011 at 15:03just to keep it simple, Apply a low level voltage in NRST pin then High level voltage your micro will reset, and enjoy it
Posted on May 17, 2011 at 15:03the instruction (u16)(((u16)TIM1->CNTRH << 8) | (u16)(TIM1->CNTRL)) In my opinion has Two side the left side and Right side and the compiler according to its rules of converting to assembly will begin from the right or...
Posted on May 17, 2011 at 15:03Hi, I suggest to to try another Quartz for the Eval or it can be badly insert, because When you say that Eval is freezing or reboot, it's means that the system doesn't find any Clock source to execute instructions so t...
Posted on May 17, 2011 at 15:03Hi Matti_69, You should n't replace your micro, As Mozra said it's a normal behaviour for STM8S, and I want to add that for debug purpose SWD must be set to 0 and If you want to use the PD1 pin (Swim pin) you must just...