Hello,The X-NUCLEO-SRC1M1 is a Nucleo expansion board that can be added on top of any Nucleo-64 board when your bus voltage is 5V. If you want to implement fast charging, you'll need a Nucleo-64 board that supports UCPD (USB-C Power Delivery) like NU...
Hello,The shield TCPP03 is X-NUCLEO-DRP1M1 Nucleo Expansion Board where the TCPP03-M20 is used as a USB Type-C Port Protection for overvoltage and overcurrent protections. This Nucleo Expansion Board uses the X-CUBE-TCPP as Software Expansion where a...
Have you had a look into X-CUBE-TCPP to request voltage from USB-PD SOURCE? This example code will facilitate the Power Delivery PDO negotiation between the sink and the source. You can request any PDO up to 100W using X-NUCLEO-USBPDM1 or the X-NUCL...
Hello, The X-NUCLEO-USBPDM1 allows to negotiate PDOs using Power Delivery.Now, with the X-NUCLEO-SNK1M1 and X-CUBE-TCPP you can also request voltage from USB-PD SOURCE using STM32G0B1RE as a SINK.Additional feature in X-NUCLEO-SNK1M1 is that you can...