User Activity

Board: NUcleo 64-G474  I just want to read 2 channels of an ADC but am presented with a bewildering array of incredibly confusing options: Ranks, Continuous mode, discontinous mode, number of conversions, oversampling, triggers, etc, etc, etc. The em...
I'm having trouble understanding what the instruction below wants me to do..... It says: "Solder R47". -On which board?-Solder it where?-What value is the resistor?    
Motor control workbench Version: 6.2.0STM32CubeMX Version: 6.10.0STM32CubeIDE Version: 1.14.0Controler: NUCLEO64-STMG431RBDriver: IMH07M1Motor: rs2205: very simmilar spec to Bullrunning motor (7PP, 0.1ohm, 0.01mh, etc....) Hi. I created a FOC app wit...
It's a pretty common need in an IDE to be able to branch or "fork" a project. Normall, I'd make a copy of the projet at the file level, then rename the original and continue development on that. However, Ranaming a project not only crashes, but also ...
Hello, I'm trying to use my B-G431B-ESC with the 6-step algorithm. I''ve tried with a coupld of profiled motors and what happes is that it starts up fine, but after ~2K RPM, the motor starts to squeel and lose power. I feel like this has something to...
Kudos from