Hello,I installed all needed tools and software according to STM32H5_Security_Workshop_tools_installation.pdf but I cannot compile the SMAK application. This is the error message I get: Br,Iulia
Hello,I am new to ST and I need some advice. I need to create two pwm signals that are synchronized. PWM A should go to a physical channel and PWM B which runs at half the frequency is supposed to trigger ADC conversion at falling edge. The signals a...
I have mentioned in this thread already that I have followed the STM32H5_Security_Workshop_tools_installation.pdf and I have also attached screenshots to this thread that I have installed STM32Cube_FW_H5_V1.1.1 according to the pdf.
I confirm I have done these steps. I have tested opening the project both from "C:\STM32Cube_FW_H5_V1.1.1/..." and "C:\Users\username\STM32Cube\Repository\STM32Cube_FW_H5_V1.1.1..." with the same result. In both cases I have copied the postbuild.bat ...
The only thing that might differ is this requirement:STM32Cube_H5_V1.1.0 with STM32Cube_H5_V1.1.1 patch, or laterI installed this according to the instructions in the pdf file provided:How can the IDE not find the env.sh file even though it's there? ...
Yes, exactly, I don't have a prebuild.log file in C:\STM32Cube_FW_H5_V1.1.1\Projects\STM32H573I-DK\Applications\ROT\SMAK_Appli.I seem to have a prebuild.log file directly under the C:\ but it doesn't provide more information than the STM32CubeIDE co...