User Activity

Hi,I access the system bootloader by setting the bits nBOOT0/nSWBOOT0 = 0 and nBOOT1 = 1 in my code. I manage to connect via UART and flash my new firmware but then my MCU does not reboot because it remains in the system bootloader. How can I do this...
Hello,I having an issue with the LSM6DSL. It's doesn't trigger interruptions on INT1 or INT2.I'm working with the STM32WB10CC and I'm connected through SPI to the LSM6DSL. The SPI is working I'm able to communicate with the sensor but it's not trigge...
Hi,I'm working on STM32WB10CC with 320KB of flash memory.I'm using the full ble stack 1.14.1 (stm32wb1x_BLE_Stack_full_fw.bin) which has a size of 148KB.In the release note it's written you have to put it at this address 0x08021000.If I'm doing the m...
Hi,I'm looking for the max size of SRAM allocated for the GATT database for the STM32WB series.I've found the informations for WB55 and WB15 but I can't find the information for WB10/30/35/50/. Does anyone know these values or how it can be calculate...
Hello, I'm trying to flash my STM32WB15CC using UART1 without using pin BOOT0(PH3). I'm using a NUCLEO-WB15CC. For that I know that I've to set some bits in OPTR register and jump from application code to memory system bootloader and then connect to ...
Kudos from