Posted on July 10, 2014 at 11:11The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on July 14, 2014 at 19:35Hi bs How are you running the I2S port? master/slave? receive/transmit? Who is the second stream? You are running full-duplex? or both I2S ports? Are you running on internal or external clock for the I2S MCLK? Maybe y...
Posted on July 13, 2014 at 18:41Ok, the problem continues. The big capacitor added didn't solved the issue. The ''shift'' still occurs, but now I have to wait even longer to happen. But I'm on the right track. So there are two clock domains which ne...
Posted on July 12, 2014 at 14:33You are right. I took this option as a backup. However. Today I figured it out The ''shift'' problem is because of my power source. If I short-circuit the power for a very very short time before the voltage regulato...
Posted on July 11, 2014 at 17:27 Hi bs 1) SRC4392 can be set to run with 12.288Mhz or 24.576Mhz oscillator. The only thing depends is how you set the internal clock divider inside Port A/B by using I2C protocol. I have a crystal oscillator(TCXO 12....