User Activity

I have a project running on my Stm32H7. I imported my ethernetif/lwip settings from the Stm32CubeH7 H723 lwip + freertos http server example, but made some small changes. For the most part in the most basic sense, the driver works and my board at lea...
I have an STM32h723, connected to the STM32CubeProgrammer via SWD. My flash image is 136672B in size and contains code to read the entire flash image, SHA3 it, and then compare that SHA3 to an SHA3 which is located, via linked script + post build scr...
Kudos from
Kudos given to