User Activity

Hello everyone !I've recently hit a snag in a motor FOC project of mine: the CORDIC unit on a STM32G431xB doesn't give out similar q1.15 results when the input are 32 and 16 bits.In the current setup, both sine an cosine coefficient are pre-stored as...
Used ecosystem :STM32CubeIDE version: 1.4.2 Build: 7643_20200813_1322 (UTC)TouchGFX vesion 4.5.0 , with STM32F746G-DISCO template version 3.0.2STM32Cube FW_F7_V1.16.0 DriversTo repeat the issue :1) Create a new project using TouchGFX Editor, using ST...
Posted on May 18, 2017 at 22:46Hi.I'm trying to use TIM1's channel 1 as a spindle RPM input capture. ( device is STM32F103C8 )Knowing that the spindle has a single pulse per revolution and is rated from 0 to 30K rpm, the frequency domain is 0 to 500...
Kudos from
Kudos given to