hi,i want to flashing to flash but i have a problem If the flash is not entering memory map at all , the flashing is workingif memory map was activated, even once, the flashing is failing
hi,i use stm32h743 and i use emwin functions ,but the functions of GUI not working i asked segger and they said maybe we need to update my version my version is: GUI_VERSION 54401do you have newer version ?
We are using stm32H743 We need a frame buffer of 150K to our LCD. we do not have an external RAM, so we use the 412K internal RAM.We also work with USB (Full speed mode).each peripheral work on it own , but not together. if we enable both of them the...
We are using stm32H743We need a frame buffer of 150K to our LCD. we do not have an external RAM, so we use the 412K internal RAM.We also work with USB (Full speed mode).each peripheral work on it own , but not together. if we enable both of them they...
hi, i downloaded this version but the problem is still here i tried to compile the function GUI_LoadCSVEX() and i didnt success i got hard faultthis is the hard fault:<exception frame>[__aeabi_memcpy4 + 0x5][_GetData2 + 0x25][_GetCharBuffered.constpr...
hi,from where i can take the version of st/emwin i want to downlaod the new version from your websiteand there is cube that create emwin cause my cube didnt create the emwin we did it ourselvesthanks,hadar