User Activity

Hello all,I was wondering if there was a way to output the sensor values from the sensortile box to the serial monitor such as Putty. I wanted to use Processing3 along with the serial data to make my own graphical solution.I am aware that the Unicle...
So I wanted to use the X-CUBE-MEMS1 library for the SensorTile module but noticed that the projects were made for the IKS01A1 and the IKS01A2 boards. Which one of these projects/boards would I need to select for the SensorTile application?
Playing around with the sensortile and the senortile box has been fun. However I wanted to go beyond the given firmware packs and even combine a few of them (BLE, AI and MOTION firmware packs) to build a project for my own application.I am pretty new...
Hello All,I recently came across the MotionFX library as part of the FP-SNS-ALLMEMS2 function pack and was delighted to find all additional functionality that could be added to the Sensortile box. While the above mentioned function pack is amazing I ...
Hello All,I have been planning on a project around the sensortile box. For this project I wanted to use multiple sensortile box modules and have each of them send their heading directions via bluetooth to a master PC or a HUB.I am aware of the FP-SNS...
Kudos from