User Activity

Hello,I'm working on a new project in which I'm using the new STMG series for development. At present, I'm trying to program the controller via JTAG. Unfortunately, the ST-Link is not able to connect to the controller. I'm attaching the screenshot of...
Hello,I'm working on a project, wherein I've interfaced my STM32L433 controller with a Flash-IC (Nor flash) on the SPI port. At present, there is continuously bulk reading and writing operation is going on. Due to random power-cut, some of the flash ...
Hello!I'm starting to work on a project and it is built on the IAR IDe (the controller is stm32f103rct6). My task is to change the IDe (to Keil) of this existing project. After reviewing the existing code, I noticed, few configurational structures ar...
Hello,I'm working on a NUCLEO-G474RE board (using the LL libraries available on ST site), and I came across an issue, the USART3 available on the PB10 and PB11 is not working. I tried to generate the same code from the CUBEMX as well but unfortunatel...
Hello, I'm working on a project based on STM32F446 controller. In my project, I'm reading and writing some data on the external flash. Its interface to one of the SPI port of the controller. The frequency of data accessing (reading and writing) is a ...
Kudos from