User Activity

Are there any samples I can order? I don't see it listed on any of the distributor sites. If anyone knows where I can get one that would be great! Also, if an ST rep can state when they will be available to order that would also be great! Thanks
My design is using an LD1117S33CTR voltage regulator. I am experience some rather odd behaviour where the regulators output is actually increasing from the expected 3.3V all the way up to 4V. What could cause such behaviour? I am stumped.
The SetupSTMCUFinder-4.0.0-RC3 file can be clicked, and it seems like my OS tries to open / run it, but ultimately nothing happens. I remember having a similar issue with another piece of stm software, and remember running some command in the termina...
I have an application running on an STM32F4 which uses the STM32 HAL framework + FreeRTOS. I occasionally need to store some settings in flash during runtime and have written the following function to erase the data at my target address of 0x08060000...
I have been working on a configuration which will allow me to detect the frequency of an external square wave, and then divide the periiod of the signal into smaller segments for executing code. I didn't mean to post this yet, just wanted to save as ...