User Activity

Hi,I hope everyone is fine.I have question about Inheritance Certification.The Thread Group says;The Thread Group allows certification by inheritance for families of end products that reuse the same Thread system (chip and stack) and the same use cas...
Hi, HAL_UART_STATE_BUSY_TX is always Set when I change the ClockPrescaler of USART Paremeter.My Cube configurations are in photo above. I have to drive Usart with 100 Baudrate. Systemclock Frequency is 50Mhz.  When SystemClock is 50Mhz and ClockPresc...
My PWM and DMA configurations shown in below image and I wrote a simple code to start pwm.  As you see below, I set a gpio output pin and after that pwm starting. PWM period has setted to 20ms. What I except, I except start pwm after a few us gpio ...