User Activity

HelloI use CAN FD and have a functioning communication with 3 participants. Now I want to activate the interrupt that notifies me when the device has lost the arbitration contest. I forward each of the four NVIC interrupts in stm32h7xx_hal_fdcan: voi...
Good afternoonI am working on the STM32H755 and am dealing with the retransmissions from my CAN FD periphery. According to the ISO-11898-1:2024 standard, the number of retransmissions should be configurable:"- from 0 (no retransmission),- to at least...
Hello,Where can I find documentation on the error counters of the FDCAN_ErrorCountersTypeDef structure? I would be particularly interested in how the incrementation of TxErrorCnt behaves if hfdcan1.Init.AutoRetransmission = ENABLE; (How often does th...
Hello, I am looking for the BSDL files for the processors of the STM32H757I-EVAL board and the STM32H755 processor. Thanks in advance!
For a specific task at my workstation, I need to cache a variable before the watchdog reset and query it again after the reset. For this I have implemented a timer that writes the variable to RAM just before the watchdog. For this I defined according...
Kudos from