User Activity

Hello everyone, I am using a custom board with STM32H750 and I am trying to develop a file system with FILEX. The file system' s media is a uSD card with 10 MB/s baudrate which is communicating with the micro thanks to the SDMMC peripheral. The SDMMC...
Hello everyone, I am using a STM32H750 with STM32CubeExpansion_Audio_V1.1.1 and I am trying to use the Graphical equalizer library.This is what I've done: I have an aux audio signal that I'm sampling at 96Khz with a DMA's interrupt transfer every 1 m...
Hello everyone, I am using STM32H7S78-DK with TouchGFX HVAC-IoT Demo and I am encountering some problem while I am trying to debug application project. I can flash my code but I can't debug it.Can anyone tell me which is the problem?I am using TouchG...
Hello everyone, I bought a STM32H7S78-DK and I am having problems with it. After playing with it a bit, I decided to flash the original firmware which I can download from ST official site (the name of the project's folder is "STM32H7S78-DK TouchGFX D...
Hello everyone, I am using a custom board with a STM32H750VBT6 and TSC2046 Touch Screen Controller with resistive screen. Unfortunately, I am experiencing some troubles with the swipe gesture due to the nature of resistive screen (sometimes the touch...
Kudos from