User Activity

hi,i would like to disable the uart debug console so that i can use uart4 for something else. how do i disable the console?thanks,vince
hi,we are using usart1 to communicate w/ a device using custom baud rates. we have it working but sometimes we don't get all of the data that is sent by the device. it one or two bytes are dropped at the beginning of the message or there are severa...
hi,we are trying to flash our yocto build on our custom board using the stm32cubeprogrammer via usb in dfu mode. the flashing fails w/ the following message:19:33:39 : Opening and parsing file: tf-a-stm32mp157f-nff-mx-usb.stm3219:33:39 :  File      ...
hi,we are going to use the STPMIC1E in our design but bc the part is not available we are going to use the STPMIC1B for the initial boards we produce and then change to the desired part.however, the buck4 regulator needs to be changed to 1.2 volts fr...
hi,i would like to be able to control the pmic from user space. everything that i have read in the stm documentation indicates that it is not possible to do this. the sysfs interface is read only. i would like to be able to access the consumer dri...