Hi Rob, how did you perform the measure? And did you have the possibility to use a reference thermometer to check if the drift is due to the device or to environmental factors? And how many samples did you measured? Maybe the thermal inertial resista...
Hi Anton,It probably depends on the accuracy you need. As a general overview about the parameters (angle, frequency...) affecting the accuracy you might see this application note --> https://www.st.com/resource/en/application_note/an5551-precise-and-...
Hi,Please consider this sentence:In order to enable the embedded functionalities of the ISM330DLC , the FUNC_EN bit of the CTRL10_C register has to be set to 1; after enabling the embedded functionalities, the MASTER_CONFIG register has to be used fo...
Hi, usually they are driven or left at high impedance, so the capacitance is mostly determined by the parasitic of the pcb on the I2C lines.Pay attention to the max I2C speed. I believe you can go up to 100kOhm pullup, if you want to minimize the con...
Hi,a standard for the Gyroscope characterization (and calibration) is the rate table, such as these ones produced by Aerosmith.https://www.ideal-aerosmith.com/products/1-2-or-3-axis-rate-and-positioning-tables/It is a standard in many laboratories. T...