OŞeno.1
Associate II
since
2021-07-02
2023-06-14
User statistics
8
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About OŞeno.1
Options
Report User
User Activity
Posts
Replies
I am using STM32L443 processor. When the processor is locked, I reset the processor with NRST with external wdg. The processor is not reset although WDG is working properly.
2022-11-29
I checked WDG. The system is working properly. If there is no reset, it resets when I disable the WDG signal. In case of deadlock, I pull to GND myself, but it still does not reset. The only solution is to cut off all energy.
I am using stm32l443 mcu. When the processor is locked, the processor does not work even though I trigger it with an external wdg. Everything is correct in the circuit design. If the NRSTe is triggered while the system is running, it resets.
2022-07-17
Re: I am using STM32L443 processor. When the processor is locked, I reset the processor with NRST with external wdg. The processor is not reset although WDG is working properly.
2022-12-20
what is the content of the project
Re: I am using STM32L443 processor. When the processor is locked, I reset the processor with NRST with external wdg. The processor is not reset although WDG is working properly.
2022-12-20
I couldn't find any relevant information.
Re: I am using STM32L443 processor. When the processor is locked, I reset the processor with NRST with external wdg. The processor is not reset although WDG is working properly.
2022-12-20
Sorry, I still haven't found anything clear. But upon the information I received, I was told to define the idle pins as outputs, I will try.
Re: I am using stm32l443 mcu. When the processor is locked, the processor does not work even though I trigger it with an external wdg. Everything is correct in the circuit design. If the NRSTe is triggered while the system is running, it resets.
2022-07-18
Re: I am using stm32l443 mcu. When the processor is locked, the processor does not work even though I trigger it with an external wdg. Everything is correct in the circuit design. If the NRSTe is triggered while the system is running, it resets.
2022-07-18
BOOT0 pin connected gnd. HSE oscillator
View more