User Activity

Hi,From the errata sheet I have seen, that the STM32F7x2 has a problem with the cache in write through:Errata:https://www.st.com/resource/en/errata_sheet/es0360-stm32f72xxx-and-stm32f73xxx-device-limitations-stmicroelectronics.pdfDatasheet:https://ww...
Hi,I have seen, that for the bootloader with just one image, it is only possible to use the YMODEM with UART for updating the firmware with the SBSFU. Now what I'm am concerned about is, that the YMODEM seems not to be very error tolerant. So, what f...
Hi,I have a bit trouble understanding the two keys in the SBSFU and which pairs is actually used. From AN5056, chapter 5 there is stated how to generate the two different methods and the AES key I could successfully adjust. With the ECCKEY method and...
Hi,When I have a look at the AN5056(https://www.st.com/resource/en/application_note/dm00414677-integration-guide-for-the-xcubesbsfu-stm32cube-expansion-package-stmicroelectronics.pdf), there is a possibility on page 39 to improve the boot time. That ...
Hi,I try to use the SBSFU in a project with a STM32F722 and so far it works to flash an initial firmware. Now what I would like to do is to update the firmware and for that, since I can only use one image because of the limited flash size, I corrupt ...
Kudos from