I am using I CUBE LRWAN 2.0.0STM32L072-LRWAN1 board is in use.You want to use the TRACE function UART1 (PA9, PA10) pin.The TX outputs letters to the serial, but the RX function, such as keyboard input, does not work.NVIC is also set in UART1 INIT.HAL...