User Activity

I tried upgrading the firmware on the STM32 F446RE board by accessing the usb-dfu. I used DFU-UTIL library for it. But as it turns out, we won't be able to upgrade the firmware using usb-dfu if the code already present on the board has UART or SPI or...
I was using USB-DFU for uploading LED related codes on STM32F446RE but then I came across bootloader selection flowchart which I am attaching with this question. According to this flowchart, I won't be able to access the bootloader mode in presence o...
How can I upgrade the firmware of STM32F446RE Nucleo board using USART bootloader from Linux? I have successfully upgraded firmware using USB-DFU using dfu-util library that is present for Linux but I want to do the same through USART. How can I do t...
I was using USB-DFU for uploading LED related codes on STM32F446RE but then I came across bootloader selection flowchart which I am attaching with this question. According to this flowchart, I won't be able to access the bootloader mode in presence o...
I am using dfu-util library to update firmware of STM32F446RE using Raspberry Pi as host for running dfu-util. How can I detach the target STM after I am done uploading the firmware? There is a command present in dfu-util package for detaching the ta...
Kudos from